Part Number: MSPM0G1107
Hello,
The TRM for the G series indicates that some MSPM0G devices have support for multi-word flash writes (up to 8 words at 64 bits each). The datasheet is not clear on whether or not this is implemented on the MSPM0G1107.
Does this device support multi word flash writes? It would be helpful in the datasheets to be explicit on which features described in the TRM are actually implemented on the device and which ones are NOT. Omission can be interpreted as somewhat ambiguous since it's unclear whether it's just a mistake, or if the device actually doesn't implement the feature. The way this is described is CIRCULAR where the TRM references the datasheet for specific implementation, and the datasheet references the TRM for full description. There is no definitive place where it describes what's implemented on which device!!


Munan