Part Number: AM2432
Other Parts Discussed in Thread: TPS65219
HI experts,
My customer is using TPS65219 to power AM243x, they find that powering the ADC would cause the PMIC to fail, below are details
case 1:
PMIC(1.8out) --NC--> VDDA_ADC0
AMP -> ADC0_REFP
In this case, VDDA_ADC0 is 1.9V and ADC0_REFP is 1.78 V. The other rails works normally and am243x can be powered up normally.
case 2:
Connect PMIC 1.8 out to VDDA_ADC0. In this case, VDDA_ADC0 is 1.8V, but rest of the rails fails, am243x can not be powered.
Any idea what's the cause of this?
Regards,
Hang.