Part Number: TM4C1290NCPDT
I'm trying to just generate a 1KHz 50% duty cycle signal stream, in the TM4C123 series I used a timer but can't do that with this chip (unless I had the timer generate an interrupt for each transition) but should be able to using a PWM generator. My code is as follows:
GPIOPinTypePWM(GPIO_PORTF_BASE, 0x01);
GPIOPinConfigure(GPIO_PF0_M0PWM0);
PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN | //
PWM_GEN_MODE_NO_SYNC ); //
PWMClockSet(PWM0_BASE, PWM_SYSCLK_DIV_16); // 1250KHz Clock.
PWMDeadBandDisable(PWM0_BASE, PWM_GEN_0); //
PWMOutputUpdateMode(PWM0_BASE, PWM_OUT_0_BIT, PWM_OUTPUT_MODE_NO_SYNC); //
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, 625); // 1KHz output (?)
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0, 312); // 1KHz output (?)
PWMGenEnable(PWM0_BASE, PWM_GEN_0); //
The clock is 20MHz.
Thanks,
Doug