Part Number: AM2634
Tool/software:
Dear Team,
I want to perform fast memory read/write operation, for that i want to use Memory map mode,
So kindly let me know how to use QSPI memory as Memory map mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2634
Tool/software:
Dear Team,
I want to perform fast memory read/write operation, for that i want to use Memory map mode,
So kindly let me know how to use QSPI memory as Memory map mode?
Hi vikas chaudhary,
By default the Flash reads are done in memory map mode. You can use the Flash_Read APIs in the SDK.
Best Regards,
Aakash
Dear AAkash,
What is expected time to read 1KB data at 100 Mhz clock speed in quad mode?
As pe my calculation it should be approx. 40usec,
Please confirm for the same
Hi vikas chaudhary,
There are many variables in the same.
1. QSPI clock is only supported at 80MHz on AM2634 device.
2. What is the mode in which this is configured ? Is it 1s-1s-4s mode ?
3. What is the dummy cycles required by the flash for the same ?
4. Are you looking for a performance with DMA or without DMA ?
Best Regards,
Aakash