Part Number: AM2434
Other Parts Discussed in Thread: TMDS64EVM, TMDS243EVM, LP-AM243, SYSCONFIG
Tool/software:
Does the ICSS firmware support CRS and COL inputs for half-duplex in DUAL MAC and MII modes?
If so, how should the MCU+ SDK be modified for half-duplex in DUAL MAC and MII modes?
If not, is there a firmware that supports half-duplex in DUAL MAC and MII modes?
Our customer is trying to achieve half-duplex communication (10BASE-T1S) in DUAL MAC and MII modes based on the following example project in the MCU+ SDK.
AM243x MCU+ SDK 09.02.00.50: Enet Lwip ICSSG Example
C:\ti\mcu_plus_sdk_am243x_09_02_00_50\examples\networking\lwip\enet_lwip_icssg\am243x-lp
They are testing between two AM2434 prototype boards, but a frame length is limited to 128 bytes when the CRS input is enabled.
Best regards,
Daisuke