Part Number: AM2732
Tool/software:
HI:
we use the demo project of mibspi_loopback_dma_am273x-evm_r5fss0-0_freertos_ti-arm-clang to cfg the TJA1145 cantrancv.
comment the code status = MIBSPI_enableLoopback(gMibspiHandle[CONFIG_MIBSPI0],loopback); to disable loopback function
and we find the TX and RX data right on the spi miso and mosi bus.but err in RXSRAM.
Another experiment do not comment the code status = MIBSPI_enableLoopback(gMibspiHandle[CONFIG_MIBSPI0],loopback); enable loopback function,the RXSRAM data is right.
in addition ,the e2e case about pmic I request before. use the same demo project and the spi used as mibspib, it's useful.
chang the Macro definitions and variables as follows:
#define APP_MIBSPI_MSGSIZE 10
uint16_t gMibspiTxBuffer1[APP_MIBSPI_MSGSIZE];
uint16_t gMibspiRxBuffer[APP_MIBSPI_MSGSIZE];
uint16_t gMibspiTxBuffer[]=
{
// 0x03ff, // Reg 1 Mode control
0x1400, // Reg:0x0A Lock control. Spi write access enable
0x0207, // Reg 1 Mode control
0x03ff, // Reg 1 Mode control
0x03ff, // Reg 1 Mode control
0x0204, // Reg 1 Mode control
0x03ff, // Reg 1 Mode control
0x03ff, // Reg 1 Mode control
0x0207, // Reg 1 Mode control
0x03ff, // Reg 1 Mode control
0x03ff, // Reg 1 Mode control
};
memory:

syscfg :
spi bus:
3Q.