This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Which SPI port can be used for SPI boot ?

Part Number: AM2434

Tool/software:

Hi,

My customer is now considering 2-chip solution with two AM2434s.

I'm about to recommend them to use SPI boot from Device 1 to Device 2 instead of UART boot due to the errata i2371. In this case, which SPI port can be used on Device 2 ?

Thanks and regards,
Hideaki