Part Number: UNIFLASH
Other Parts Discussed in Thread: CC2640R2F, CC2340R5
Tool/software:
Hi,
I'm facing the issue "Failed: Target must be connected before calling the function".
This issue occurs when using Uniflash CLI to flash a device in testbench by connecting target CC2640R2F with a TI Launchpad.
It is not connection issue as I'm able to use the Uniflash GUI and flash/read target without problems. Below is the command line used (Ubuntu 22):
<path to dslite.sh> --mode noConnectFlash --config=<path_to_ccxml file> --flash <path_to_FW> --verbose
Note: I tried both with power supply from Launchpad and with external power supply but I got the same error message
Does somone already faced this issue ? Is there something i can do to fix it ?
Best regards,
Antoine Bricard