Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
Hi!
I am unable to find out why the RTI Interrupt is not occuring. I basically want a 1ms timer in my code which I can use for timing events. My code is simply:
int main(void)
{
/* USER CODE BEGIN (3) */
systemInit();
/* Vector Interrupt Module Initialization */
vimInit();
/* Timer Initialization */
rtiInit();
rtiStartCounter(rtiREG1, rtiCOUNTER_BLOCK0);
rtiEnableNotification(rtiREG1, rtiNOTIFICATION_COMPARE0);
while(!(rtiREG1->INTFLAG & rtiNOTIFICATION_COMPARE0));
/* Serial Communication Initialization */
sciInit();
/* Forever Loop */
while(1)
{
/* Dummy code to transmit SCI data */
/* Buffer formation for data transfer */
Mucaa_data_ptr[0] = 0xAA;
Mucaa_data_ptr[1] = 0x01;
Mucaa_data_ptr[2] = 0x02;
Mucaa_data_ptr[3] = 0x03;
Mucaa_data_ptr[4] = 0x04;
Mucaa_data_ptr[5] = 0x05;
Mucaa_data_ptr[6] = 0x06;
Mucaa_data_ptr[7] = 0x55;
if((uint16)(Rti_ui_1ms_tmr - Mui_tx_cntr) > 2000)
{
Mui_tx_cntr = Rti_ui_1ms_tmr;
/* Enable the SCI transmit interrupt for SCI3 module */
sciEnableNotification(sciREG3, SCI_TX_INT);
/* Transmit data */
sciSend(sciREG3, 8, &Mucaa_data_ptr[0]);
}
}
/* USER CODE END */
return 0;
}
I just intend to transmit SCI data every 2 seconds, for which, I need RTI timer. Unfortunately, I am unable to attach my halcogen file for reference and therefore put the images. The variable "Rti_ui_1ms_tmr" is configured to increment in the function "rtiNotification" as follows:
void rtiNotification(rtiBASE_t *rtiREG, uint32 notification)
{
/* enter user code between the USER CODE BEGIN and USER CODE END. */
/* USER CODE BEGIN (12) */
Rti_ui_1ms_tmr++;
/* USER CODE END */
}


Regards,
Chetan.