Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I'm trying to get BiSSC working on our AM2432 (ALV package) based custom board. On our board the RS422 transceivers are connected as follows:

Our software is based on MOTOR CONTROL SDK 9.02.09 with Sysconfig 1.20.0.
In Sysconfig I'm able to select PRU_ICSSG0_PRU1 and the balls W2, T6, and Y2 for TX, RX, and CLK respectively.
My problem is the choice for the transceiver DATA_EN signal (ball V3).
I have had a look at the BiSSC examples from the SDK. They have checked the "Booster Pack" Checkbox in Sysconfig which, apparently, enables an entry field for the DATA_EN signal.
Now my question: How do I select the pin for the DATA_EN signal for our custom board?
Best regards
Johannes