Part Number: TMS570LS0432
Tool/software:
i have two different Appications in Flash at the same time , which have their own sub functions in it can i call or run those from one of the application.
the problem i am facing is if i give the starting address of application it is getting into the prefetch entry or undef entry .if i give _c_int100 function address also same issue .so ,how can i acheive jump application or if i just want to use the function in their application is it possible?

entry i will share the screen shot .