Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software:
Hello,
I am using a TM4C1294NCPDT processor and TI-RTOS. I am trying to set things up to update firmware over ethernet using the ROM based EMAC bootloader. I have successfully done this in the case of dynamic ip addresses but my application requires a static ip address; that is the processor is set up to use a static ip address. When the processor is using a dynamic address the ROM bootloader works great. When I try to use a static address the LM Flash Programmer application never connects. Is there a way to get the ROM based bootloader to work in the case of static ip addresses?
Thanks
Scott Bates
.