Part Number: LP-MSPM0L1306
Other Parts Discussed in Thread: LP-MSPM0G3507, MSPM0G3507, MSPM0L1306
Tool/software:
Hi M0 team,
I'm attempting to use the secondary_bsl_uart example from the M0 SDK onto an MPSM0G3507 launchpad, but am encountering the following issue.

Using the following thread, I was able to change the Debugger to allow erasing of NONMAIN before writing.
However, debugging now causes a new error:

From this point i have to factory reset the board with the following tool, which allows me to at least connect to the target.
https://dev.ti.com/gallery/view/TIMSPGC/MSPM0_Factory_Reset_Tool/ver/0.0.3/
However, repeated attempts to load through the debugger continue to fail. Any thoughts?