This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1107:Two app firmware flashing problem

Part Number: MSPM0G1107
Other Parts Discussed in Thread: MSPM0C1104

Tool/software:

你好,

我有兩個APP代碼需要 編程 到同一個晶片中。我可以調整擦除方法來實現此目的嗎?

應用1 應用2

 ------

和我的兩個APP(.map)

目前,將 APP1 寫入快閃記憶體會導致 (M0G1107) 出現下列錯誤:

CORTEX_M0P:快閃記憶體編程器:位址 0x20000 處的磁區 80 擦除失敗
CORTEX_M0P:錯誤:(錯誤 -1001 @ 0x0)此裝置不支援要求的操作。 (仿真包12.7.0.00130)

我是否缺少任何設定?謝謝。

  • Revision  APP1 

  • If you want to program two different application code into the chip at the same time, you need to define the two application code in different memory. The cmd file must be changed in the two different application's project to define which memory it is located. You can't use the same cmd file for the two application code that will make the application address conflicted.

  • Hi Gary Gao

    I have cmdA and cmdB documents.They are  different projects

    cmdA                                                                                                   cmdB

    I Flashing cmdB will result in an error.

    error code

    CORTEX_M0P: Error: (Error -1001 @ 0x0) Requested operation is not supported on this device. (Emulation package 12.7.0.00130)
    CORTEX_M0P: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.7.0.00130)

  • Due to app B is not start from 0x00, the MCU will go into 0x00 when start up due to all the values are both 0xFFFF, so it will hang up and the error above. If you want to debug app B, you can put it at 0x00 first when you finished the debug then you can move it to other address.

  • Thank you for your response. I encountered an error during the flashing process (although it's working fine now). Currently, I can successfully flash the firmware, but if I try to flash appB it again, an error occurs. The only way I can flash it again is by performing a "MSPMO_MassErase_Manual" function first.

    The settings for my app B are as follows:

    error code

    CORTEX_M0P: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.7.0.00130)
    CORTEX_M0P: Unable to determine target status after 20 attempts
    CORTEX_M0P: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    CORTEX_M0P: File Loader: Memory write failed: Could not read 0x20200014: target is not connected
    CORTEX_M0P: GEL: File: C:\Users\1130512\Documents\work1\TI_workspace\em_T1107T\Debug\em_T1107T.out: Load failed.

  • Please choose this one

    Could you help to provide the TI-TXT format firmware of the two application code to me? Let me check if any address conflict 

  • Thank Gary Gao

    This is my app. TXT file.em_T1107T.txt

    @0000
    00 40 20 20 D1 0F 00 00 AF 08 00 00 AF 08 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 AF 08 00 00 
    00 00 00 00 00 00 00 00 AF 08 00 00 AF 08 00 00 
    AF 08 00 00 AF 08 00 00 AF 08 00 00 B1 08 00 00 
    AF 08 00 00 AF 08 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 AF 08 00 00 AF 08 00 00 00 00 00 00 
    00 00 00 00 AF 08 00 00 AF 08 00 00 AF 08 00 00 
    05 0C 00 00 AF 08 00 00 AF 08 00 00 AF 08 00 00 
    AF 08 00 00 AF 08 00 00 00 00 00 00 00 00 00 00 
    AF 08 00 00 AF 08 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 AF 08 00 00 AF 08 00 00 
    10 B5 4C 48 00 24 04 80 4B 48 04 80 4B 48 04 80 
    4B 48 04 80 4B 48 04 80 4B 48 04 80 4B 48 04 80 
    4B 48 04 80 4B 48 04 80 4B 48 04 80 4B 48 04 80 
    4B 48 04 70 4B 48 04 70 4B 48 04 60 4B 48 01 88 
    4B 4A 14 70 4B 4A 14 70 4B 4A 14 60 4B 4A 14 70 
    4B 4A 14 70 4B 4A 14 60 07 22 91 43 01 80 4A 48 
    4A 49 01 60 4A 48 01 60 4A 48 01 60 4A 48 04 80 
    4A 48 04 80 4A 48 70 22 02 60 4A 48 04 60 4A 4A 
    13 88 4A 48 03 40 13 80 49 4A 11 60 49 49 0C 80 
    49 49 32 22 0A 80 49 49 0C 80 49 49 0C 80 01 21 
    49 03 48 4A 11 60 48 49 0A 88 80 30 10 40 08 80 
    46 48 04 80 46 48 04 80 46 48 04 80 46 48 06 21 
    01 80 46 48 04 80 46 48 04 80 46 48 04 80 46 48 
    04 80 46 48 04 80 46 48 04 80 46 48 3C 21 00 F0 
    07 FF 45 48 04 80 45 48 04 80 45 48 04 80 45 48 
    04 80 45 48 04 80 45 48 04 80 45 48 04 80 45 48 
    04 80 45 48 04 80 45 48 04 80 45 48 04 80 45 48 
    44 80 04 80 44 48 44 80 04 80 44 48 04 80 44 48 
    04 80 44 48 04 80 44 48 04 80 44 48 04 80 44 48 
    04 80 10 BD 6E 01 20 20 54 01 20 20 5E 01 20 20 
    56 01 20 20 5C 01 20 20 5A 01 20 20 60 01 20 20 
    52 01 20 20 58 01 20 20 62 01 20 20 50 01 20 20 
    AB 01 20 20 AA 01 20 20 10 01 20 20 08 01 20 20 
    AD 01 20 20 AC 01 20 20 18 01 20 20 AF 01 20 20 
    AE 01 20 20 34 01 20 20 14 01 20 20 FF FF 00 00 
    1C 01 20 20 38 01 20 20 D2 00 20 20 A0 01 20 20 
    24 01 20 20 20 01 20 20 28 01 20 20 7F FE FF FF 
    0C 01 20 20 9E 01 20 20 6A 01 20 20 64 01 20 20 
    68 01 20 20 90 32 0A 40 2C 01 20 20 70 01 20 20 
    72 01 20 20 74 01 20 20 6C 01 20 20 A2 01 20 20 
    A4 01 20 20 A6 01 20 20 A8 01 20 20 96 01 20 20 
    7E 01 20 20 96 00 20 20 8E 01 20 20 76 01 20 20 
    80 01 20 20 84 01 20 20 82 01 20 20 94 01 20 20 
    98 01 20 20 9A 01 20 20 92 01 20 20 86 01 20 20 
    7A 01 20 20 40 01 20 20 44 01 20 20 90 01 20 20 
    88 01 20 20 8A 01 20 20 78 01 20 20 8C 01 20 20 
    7C 01 20 20 F0 B5 01 88 4A 1E 03 2A 2A D8 91 00 
    01 A2 51 58 8F 46 C0 46 29 03 00 00 53 03 00 00 
    59 03 00 00 5F 03 00 00 43 49 09 88 43 4A 14 88 
    01 23 1D 02 25 43 15 80 41 4D 2A 88 57 1C BE B2 
    00 22 04 2E 14 46 00 D8 3C 46 04 2E 0E D8 10 26 
    0E E0 39 49 09 88 26 E0 37 49 09 88 31 E0 36 49 
    09 88 47 E0 05 29 66 D3 04 22 63 E0 41 26 36 01 
    2C 80 34 4D 2C 88 64 1C A7 B2 09 2F 00 D8 22 46 
    31 43 09 2F 01 D9 DC 02 21 43 2A 80 2E 4C 22 88 
    52 1C 95 B2 22 80 14 2D 05 D3 1A 03 11 43 26 4A 
    11 80 00 22 22 80 29 4A 13 88 5B 1C 9C B2 13 80 
    05 2C 04 D3 26 4B 19 43 00 23 13 80 01 E0 08 22 
    11 43 24 4A 13 88 5B 1C 9C B2 04 2C 00 D9 00 23 
    04 2C 01 D8 04 24 00 E0 1F 4C 21 43 13 80 1F 4A 
    13 88 5B 1C 9C B2 13 80 9C 42 03 D1 20 23 19 43 
    00 23 13 80 01 22 0C 46 14 43 0F 4B 1C 80 18 4D 
    2E 88 76 1C B7 B2 2E 80 0A 2F 05 D3 03 24 21 43 
    19 80 00 24 2C 80 0C 46 12 49 0D 88 6D 1C AE B2 
    0D 80 32 2E 05 D3 52 03 14 43 1C 80 00 22 0A 80 
    00 E0 00 22 02 80 F0 BD 30 01 20 20 2C 01 20 20 
    60 01 20 20 52 01 20 20 58 01 20 20 5A 01 20 20 
    08 80 FF FF 5C 01 20 20 04 40 00 00 56 01 20 20 
    54 01 20 20 5E 01 20 20 B0 B5 39 4C 21 88 C8 07 
    27 D1 88 07 2A D4 88 04 30 D4 48 07 08 D5 36 48 
    02 88 C1 23 9B 01 13 43 03 80 34 48 01 40 21 80 
    01 25 AA 03 0B 46 13 40 20 20 C0 43 58 40 08 40 
    20 32 11 42 00 D0 20 80 28 22 03 46 93 43 1A B2 
    09 07 19 D4 00 2A 17 D4 C1 06 1E D4 41 05 30 D4 
    3B E0 01 20 81 43 21 80 88 07 D4 D5 00 F0 BE FC 
    21 88 02 20 81 43 21 80 88 04 CE D5 1D 48 01 40 
    21 80 48 07 CB D4 D3 E7 00 2A 01 D4 10 46 01 E0 
    1B 49 08 40 20 80 C1 06 E0 D5 1A 48 01 88 00 29 
    03 D1 19 49 00 22 0A 80 05 80 00 F0 B5 FC 17 48 
    01 88 49 1C 01 80 20 88 10 21 88 43 20 80 41 05 
    0B D5 10 49 0A 88 01 2A 04 D1 0F 4A 14 23 13 80 
    02 22 0A 80 0E 49 08 40 20 80 C1 04 89 0F 05 D0 
    29 03 01 40 0B 4A 4A 40 02 40 22 80 B0 BD C0 46 
    30 01 20 20 FF DF 00 00 04 01 20 20 FB FF 00 00 
    D7 7F 00 00 9E 01 20 20 6A 01 20 20 50 01 20 20 
    FF FB 00 00 FF F7 00 00 B0 B5 36 4A 80 18 4A 68 
    42 60 0A 78 22 2A 56 D8 93 00 01 A4 E3 58 9F 46 
    2D 06 00 00 37 06 00 00 2D 06 00 00 37 06 00 00 
    37 06 00 00 37 06 00 00 37 06 00 00 37 06 00 00 
    37 06 00 00 37 06 00 00 37 06 00 00 37 06 00 00 
    37 06 00 00 37 06 00 00 37 06 00 00 37 06 00 00 
    1D 06 00 00 37 06 00 00 1D 06 00 00 37 06 00 00 
    37 06 00 00 37 06 00 00 37 06 00 00 37 06 00 00 
    37 06 00 00 37 06 00 00 37 06 00 00 37 06 00 00 
    37 06 00 00 37 06 00 00 37 06 00 00 37 06 00 00 
    1D 06 00 00 37 06 00 00 1D 06 00 00 03 68 03 24 
    24 07 A3 43 01 24 64 07 1B 19 03 E0 03 68 03 24 
    24 07 A3 43 03 60 0B 69 C3 60 CB 68 C4 6A 06 4D 
    25 40 06 4C 1C 40 2B 19 C3 62 09 7A 11 43 01 60 
    B0 BD C0 46 04 18 00 00 88 88 FD FF 77 77 02 00 
    F0 B5 84 B0 30 49 31 4A 01 25 AC 03 16 68 2B 02 
    03 93 9E 43 16 60 0E 68 26 42 05 D1 0E 68 26 42 
    02 D1 0E 68 26 42 F6 D0 6C 02 46 7E 97 69 AF 43 
    2E 40 BD 19 95 61 20 25 45 5D D6 69 03 27 BE 43 
    3D 40 75 19 D5 61 22 4D 2E 68 07 27 37 40 05 26 
    2E 60 46 6A 33 68 13 62 73 68 53 62 2F 60 C3 69 
    5B 06 5B 0C D5 69 7F 26 36 02 B5 43 EB 18 D3 61 
    E8 C8 00 97 07 68 01 97 47 68 02 97 1B 07 1B 0B 
    2D 03 AD B2 ED 18 33 07 1B 0D 00 7A 00 9E 35 43 
    1D 43 01 9B 1D 43 02 9B 1D 43 05 43 90 69 0D 4B 
    03 40 0D 48 28 40 C0 18 90 61 10 68 03 9B 18 43 
    10 60 08 68 20 42 05 D1 08 68 20 42 02 D1 08 68 
    20 42 F6 D0 04 B0 F0 BD 04 02 0B 40 08 01 0B 40 
    00 13 40 40 8D 00 F0 FF 72 FF 0F 00 70 B5 2B 48 
    81 21 81 67 C1 67 2A 4A 11 60 D1 60 11 61 51 61 
    91 61 D1 61 91 62 D1 62 11 63 51 63 91 63 D1 63 
    D1 64 11 65 51 65 91 65 D1 65 91 66 D1 66 01 60 
    41 60 81 60 C1 61 01 65 41 65 1E 4C 1E 4B 23 60 
    23 63 1E 4B 1E 4D 1D 60 1D 63 00 25 45 62 85 62 
    82 25 85 63 1B 4D 6E 1C C6 63 01 67 C1 66 81 66 
    01 66 41 66 81 65 C1 64 81 64 41 64 01 64 41 67 
    C1 65 41 63 01 63 C1 62 45 61 01 61 C1 60 01 62 
    51 66 11 66 91 64 51 64 11 64 91 60 51 60 81 61 
    0D 48 20 60 20 63 0D 48 18 60 18 46 10 38 07 21 
    89 02 01 60 0A 48 18 63 70 BD C0 46 04 80 42 40 
    84 80 42 40 A0 12 0A 40 0B CC E7 1F A0 32 0A 40 
    00 C0 1F 03 81 00 04 00 94 33 00 60 F3 23 E0 0C 
    F3 3F E0 0C 00 2A 49 D0 84 46 8B 07 1C D1 83 07 
    22 D1 10 2A 08 D3 70 B4 10 3A 78 C9 78 C0 10 3A 
    FB D2 70 BC 10 32 38 D0 04 2A 2C D3 08 2A 05 D3 
    0C 2A 01 D3 08 C9 08 C0 08 C9 08 C0 08 C9 08 C0 
    92 07 2A D0 92 0F 22 E0 0B 78 03 70 49 1C 40 1C 
    52 1E 22 D0 8B 07 F7 D1 C3 07 14 D1 83 07 D8 D0 
    12 1F 12 D3 08 C9 03 80 1B 0C 43 80 00 1D 12 1F 
    F8 D2 0A E0 08 C9 03 70 1B 0A 43 70 1B 0A 83 70 
    1B 0A C3 70 00 1D 12 1F F4 D2 12 1D 05 D0 0B 78 
    03 70 49 1C 40 1C 52 1E F9 D1 60 46 70 47 FE E7 
    F0 B5 81 B0 18 48 00 68 C0 B2 0B 28 0D D1 17 48 
    00 F0 2C FB 16 49 08 80 16 49 0A 88 52 1C 0A 80 
    15 4D 29 88 4A 06 92 0F 01 D0 01 B0 F0 BD 80 22 
    11 43 29 80 11 49 00 26 0E 80 11 4F 39 68 08 80 
    88 1C 38 60 0F 4C 21 46 64 31 88 42 ED D9 28 21 
    20 46 00 F0 55 FB 28 88 0B 49 0E 80 3C 60 0B 49 
    01 40 29 80 01 B0 F0 BD 20 10 50 40 00 00 50 40 
    96 01 20 20 66 01 20 20 3C 01 20 20 7E 01 20 20 
    48 01 20 20 00 00 20 20 9C 01 20 20 17 FE 00 00 
    F0 B5 81 B0 1E 48 00 24 04 60 1E 4D 28 68 0F 26 
    31 02 88 43 01 27 79 02 00 91 40 18 28 60 28 1F 
    01 68 03 22 D2 43 0A 40 02 60 68 68 B8 43 68 60 
    68 68 39 02 88 43 68 60 78 03 0A 21 22 46 00 F0 
    DD F8 11 48 FF F7 6C FE 29 68 10 20 01 43 20 22 
    91 43 29 60 69 6B 32 03 91 43 BA 03 89 18 69 63 
    29 68 3A 03 0A 43 2A 60 A9 6B 01 43 A9 63 68 6B 
    00 99 08 43 68 63 20 46 00 F0 EA F9 01 B0 F0 BD 
    08 03 0B 40 04 01 0B 40 E0 0F 00 00 00 F0 7C FA 
    00 F0 C2 FA FF F7 74 FB 18 4C 0F 20 45 03 18 4E 
    30 46 29 46 22 46 00 F0 81 FA 16 4F 38 70 30 46 
    29 46 22 46 00 F0 7A FA 13 49 08 60 38 78 03 28 
    04 D1 01 21 00 20 02 46 00 F0 28 F9 0F 4C 20 46 
    FF F7 78 FC FF F7 28 FD 00 F0 F3 F8 20 46 FF F7 
    71 FC FF F7 21 FD 00 F0 EC F8 20 46 FF F7 6A FC 
    FF F7 1A FD 00 F0 E5 F8 E9 E7 C0 46 B4 01 20 20 
    00 D0 0C 40 B0 01 20 20 4C 01 20 20 6E 01 20 20 
    F0 B5 44 1C 00 78 00 23 08 2B 30 D0 25 78 C6 07 
    0F D1 66 78 2D 01 37 09 7F 19 0F 25 35 40 ED 1C 
    12 2D 0B D1 02 25 66 57 F5 B2 00 2E 08 D4 E6 1C 
    0C E0 64 1C 4E 1C 0D 70 31 46 15 E0 A6 1C 06 E0 
    26 1D E4 78 7F 22 15 40 E2 01 55 19 12 35 09 4A 
    97 42 0E D0 FC 43 00 2D 05 D0 0A 5D 4F 1C 0A 70 
    6D 1E 39 46 F7 E7 34 46 40 08 5B 1C CC E7 20 46 
    C7 E7 F0 BD FF 0F 00 00 10 B5 16 49 16 4C 20 46 
    00 F0 5B FA 15 49 20 46 00 F0 36 F9 14 48 01 68 
    03 22 D2 03 91 43 01 60 01 69 12 4A 0A 40 41 21 
    C9 00 51 18 01 61 41 69 35 22 0A 43 0A 21 8A 43 
    42 61 41 68 01 22 11 40 43 68 93 43 59 18 41 60 
    09 49 0B 68 94 02 1C 43 0C 60 01 68 11 43 01 60 
    10 BD C0 46 29 10 00 00 00 00 50 40 1C 10 00 00 
    00 11 50 40 00 00 FF FF 28 10 50 40 F0 B5 16 4B 
    1D 46 08 3D 2E 68 01 24 A6 43 2E 60 1E 68 03 27 
    3F 03 BE 43 38 40 30 18 18 60 18 68 FF 26 B0 43 
    C9 B2 40 18 18 60 28 68 20 43 28 60 1D 68 00 2A 
    0E D0 0A 48 21 02 22 07 15 43 1D 60 02 68 0A 42 
    05 D1 02 68 0A 42 02 D1 02 68 0A 42 F6 D0 F0 BD 
    20 07 85 43 1D 60 F0 BD 10 01 0B 40 04 02 0B 40 
    84 46 83 07 06 D0 00 2A 29 D0 01 70 01 30 01 3A 
    83 07 F8 D1 04 2A 1C D3 09 06 09 0E 0B 02 19 43 
    0B 04 19 43 08 2A 10 D3 0B 00 10 2A 09 D3 70 B4 
    0F 24 16 1B 22 40 0C 00 0D 00 3A C0 10 3E FC D8 
    70 BC 08 2A 01 D3 0A C0 08 3A 04 2A 01 D3 02 C0 
    04 3A 00 2A 03 D0 01 3A 81 54 01 3A FC D2 60 46 
    70 47 70 47 10 B5 11 48 04 21 01 80 10 4A 11 88 
    49 1C 8B B2 11 80 64 2B 17 D3 03 21 01 80 00 21 
    11 80 0C 4A 13 88 5B 1C 9C B2 13 80 0A 2C 0C D3 
    02 23 03 80 11 80 08 4A 13 88 5B 1C 9C B2 13 80 
    0A 2C 02 D3 01 23 03 80 11 80 10 BD 6E 01 20 20 
    70 01 20 20 72 01 20 20 74 01 20 20 13 4B 02 28 
    05 D0 01 28 07 D1 01 20 80 02 18 61 06 E0 01 20 
    80 02 18 62 02 E0 01 20 80 02 18 60 01 20 C0 02 
    02 29 03 D0 01 29 03 D1 18 61 02 E0 18 62 00 E0 
    18 60 01 20 00 03 02 2A 03 D0 01 2A 03 D1 18 61 
    70 47 18 62 70 47 18 60 70 47 C0 46 90 32 0A 40 
    F8 B5 04 46 05 46 0C 35 00 26 0F 4F 60 88 86 42 
    17 D2 28 46 08 38 01 68 28 1F 03 68 2A 68 00 2A 
    03 D0 18 46 00 F0 78 F9 08 E0 06 48 87 42 05 D0 
    48 1C 09 78 89 00 7A 58 19 46 90 47 76 1C 0C 35 
    E4 E7 F8 BD 6C 10 00 00 60 10 00 00 70 B5 0D 48 
    40 1C 02 D0 0B 48 FF F7 D3 FF 0B 48 0B 4C 84 42 
    0C D0 0B 4D 0B 4E B5 42 08 D0 2A 68 69 68 50 1C 
    12 78 92 00 A2 58 90 47 08 35 F4 E7 00 BF 00 BF 
    70 BD C0 46 90 10 00 00 6C 10 00 00 60 10 00 00 
    7C 10 00 00 8C 10 00 00 70 B5 11 22 13 02 C2 18 
    C4 58 01 25 AC 43 C4 50 0C 88 8D 78 25 43 8C 88 
    2C 43 C5 58 08 4E 2E 40 08 4D 25 40 AC 19 C4 50 
    88 79 CB 79 03 43 08 7A 18 43 51 68 7E 23 99 43 
    18 40 08 18 50 60 70 BD E7 98 FD FF 18 67 00 00 
    10 B5 0E 49 0E 4A 01 23 5C 05 90 60 08 68 20 42 
    05 D1 08 68 20 42 02 D1 08 68 20 42 F6 D0 10 68 
    1B 04 03 43 13 60 08 68 C0 06 05 D4 08 68 C0 06 
    02 D4 08 68 C0 06 F6 D5 10 BD C0 46 04 02 0B 40 
    04 01 0B 40 10 B5 09 48 09 49 41 60 09 4A 51 60 
    09 4B 59 60 09 4C 61 60 09 49 01 60 11 60 19 60 
    21 60 10 20 00 F0 E2 F8 10 BD C0 46 00 08 0A 40 
    03 00 00 B1 00 28 0A 40 00 48 08 40 00 08 50 40 
    01 00 00 26 10 B5 08 49 08 4C 20 46 00 F0 8E F8 
    07 49 20 46 FF F7 A8 FB 06 48 01 68 01 22 11 43 
    01 60 05 48 02 60 10 BD 26 10 00 00 00 40 08 40 
    08 10 00 00 28 50 08 40 08 51 08 40 08 48 01 88 
    0A 06 0B D5 07 4A 13 88 28 2B 02 D8 58 1C 10 80 
    70 47 40 22 11 43 80 22 91 43 01 80 70 47 C0 46 
    3C 01 20 20 7E 01 20 20 06 48 01 22 91 02 12 03 
    02 62 05 4A 12 68 05 4B 9A 42 01 D1 01 60 70 47 
    01 61 70 47 90 32 0A 40 0C 01 20 20 FF FF 00 00 
    08 48 80 F3 08 88 00 BF 00 BF 00 F0 93 F8 00 28 
    01 D0 FF F7 23 FF 00 20 FF F7 88 FD 01 20 00 F0 
    8B F8 C0 46 00 40 20 20 80 B5 FF F7 83 FF FF F7 
    35 FC FF F7 35 FD FF F7 9D FF FF F7 F5 FD 02 48 
    2C 21 00 22 42 54 80 BD D4 00 20 20 B0 B5 06 4B 
    C4 18 03 25 C5 50 FF 23 10 33 23 62 E1 61 11 68 
    E1 62 00 F0 03 F8 B0 BD 04 11 00 00 82 B0 00 94 
    01 4C 01 94 10 BD 00 BF B9 01 20 20 06 49 40 18 
    01 68 49 07 05 D5 01 68 49 07 02 D5 01 68 49 07 
    F6 D4 C0 69 C0 B2 70 47 08 11 00 00 10 B5 01 22 
    12 03 83 18 0C 78 9C 60 4B 78 83 50 89 78 01 4A 
    81 50 10 BD 0C 11 00 00 01 20 00 04 03 49 08 60 
    03 48 08 22 02 60 0A 60 70 47 C0 46 00 E1 00 E0 
    80 E2 00 E0 03 22 80 58 00 28 05 D0 40 1E 4A 1C 
    00 23 0B 70 11 46 F7 E7 70 47 10 B5 01 22 12 03 
    83 18 0C 78 9C 60 49 78 81 50 10 BD 80 B5 0B 46 
    03 21 42 58 C1 1D 18 46 00 F0 0E F8 80 BD 00 00 
    0A 46 00 21 80 B5 FF F7 F3 FD 80 BD 81 1E 09 1F 
    00 BF FC D2 70 47 00 00 80 B5 FF F7 23 FC 80 BD 
    66 E7 70 47 01 20 70 47 00 BF FE E7 00 00 00 00 
    01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 10 00 00 00 00 01 00 00 07 00 00 00 
    00 00 00 00 2C 00 C4 41 02 00 00 00 27 00 00 00 
    01 00 00 00 00 00 00 00 00 00 00 00 00 00 18 00 
    00 00 00 30 00 00 08 00 63 08 00 00 00 00 00 00 
    09 49 41 18 11 22 12 02 01 23 83 50 08 68 07 22 
    10 40 04 28 07 D1 08 68 10 40 04 28 03 D1 08 68 
    10 40 04 28 F2 D0 70 47 D0 13 00 00 00 00 00 00 
    51 0A 00 00 9D 0F 00 00 75 0F 00 00 02 00 00 00 
    B1 01 00 00 00 0F 92 33 21 03 FF F0 6C 10 00 00 
    00 00 20 20 74 10 00 00 B4 01 20 20 00 00 00 00 
    0C 00 01 00 30 10 00 00 B8 01 20 20 30 00 00 00 
    q
    

    I've successfully flashed both apps now. And I want to jump between app-switching function for in-app programming (IAP). Are there any resources you can recommend?

  • You can refer to the demos in the sdk ...\ti\mspm0_sdk_2_01_00_03\examples\nortos\LP_MSPM0C1104\bsl, it has the jump functions.

  • Thanks a lot.