Part Number: AM2434
Tool/software:
Hi TI Experts,
Customer is working on AM243x SDK9.2.
They are asking if we have an open-circuit control demo (no feedback)?
Thanks,
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2434
Tool/software:
Hi TI Experts,
Customer is working on AM243x SDK9.2.
They are asking if we have an open-circuit control demo (no feedback)?
Thanks,
Kevin
hi Mukul,
thanks for your reply,yes this is related to motor control. Customer knows we have the motor control sdk, and already run some of the demo on the evm board already. Customer is asking if we have an example for the open circuit control demo which means there is no encoder feedback.
thanks,
kevin
Ok thanks for the additional background. I have reassigned to one of our Motor Control SDK experts. Responses maybe delayed as Aug 15th is a holiday for TII.
Kevin
We do not have any example with just open loop control. We have TIDEP-01032 EtherCAT-Connected Single-Chip Dual-Servo Motor Drive Reference Design which includes position and current feedback. One option is to refer to this project and build for open loop mode which does not need feedback.
If you do not need feedback, did you also consider Sitara AM26x devices. Refer to following thread for more details: (+) AM2434: AM243x - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
Regards
Dhaval