Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Bootstrap configuration for DP83822 in RMII mode

Part Number: AM2634

Tool/software:

Dear Team, 

I want to use DP83822 in RMII mode 

kindly suggest Bootstrap pins  as mention below, please fill the sheet

Required information
Pins             PU/PD                  Strap mode                     Value
COL
RX_D0
Rx_D1
Rx_D2
Rx_D3
LED0
LED1
CRS
Rx_ER
Rx_DV

Requirements
PHY1 Address                                           0x0000
PHY2 Address                                           0x0011
Mode of Operation                                     100BASE-TX, Full-Duplex, Auto-MDIX
LED0 Configuration                                    Blink Tx/Rx Activity
LED1 Configuration                                    ON for 100 Mbps SPEED
MAC configuration                                      RMII Master

Questions
1. Can we separate the link and Tx/Rx leds
2. Does speed led work in auto MDIx mode
3. How to enable auto negotiation