This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
refer to XDS110 Debug Probe User's Guide
ARMCortex-M 10-pin (CM10) and XDS110 AUX Signal
AWRL1432 circuit design connect TMDSEMU110-U Debug probe pin define as below
Please help confirm "JATG&LOG" and "AUX Signal" pin define
Thanks.
Hi Willy,
The JTAG expert is currently out of office until Tuesday 9/3, please expect a delayed response. I apologize for any inconvenience.
Best Regards,
Delaney
Hi Willy,
Thank you for your patience.
The CM-10 connections look good. The Aux board mentioned in the XDS110 Debug probe user guide: https://www.ti.com/lit/ug/sprui94/sprui94.pdf
Could you please confirm whether the J605 connector is custom connector?
Thanks.
Hi Willy,
Could you please elaborate what is the purpose of using these connections?
The AWRL1432 can be directly connected to the XDS110 Debug probe for debugging purpose, right. Why do you plan to use CC1350 launchpad which has another XDS110 chip?
Thanks.
Hi Voona
Why do you plan to use CC1350 launchpad which has another XDS110 chip?
→Sorry for the confusion , I no plan to use CC1350 launchpad
The AWRL1432 can be directly connected to the XDS110 Debug probe for debugging purpose, right.
→Yes , so required connected UART signal
CC1350 launchpad for reference only Connection method
Hi Willy,
Please correct if my below understanding is correct.
You are trying to communicate between XDS110 debug probe and CC1350 device using CC1350 launchpad via UART.
Thanks.
Hi Voona
NO, I am trying to communicate between XDS110 debug probe and AWRL1432 launchpad via UART.
no connect CC1350 require (only reference)
Please confirm with AWRL1432 circuit design connect TMDSEMU110-U Debug probe pin define.
Thanks.
Hi Willy,
Thanks for the details. For UART connectivity between XDS110 Debug probe and the AWRL6432, the UART_TX of AWRL1432 should be connected to UART_RX pin of AUX connector. Similarly, UART_RX of AWRL1432 should be connected to UART_TX pin of AUX connector. I hope this answers your question.
Best Regards,
Deexith.