Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I had an open issue (E2E AM2434: SecureBoot - appimage authentication fails - firewall configuration?), however it was not solved.
The latest recommended solution was to apply a bugfix (Fix DAC mode not enabled in ospi bootloaders).
We did apply this bugfix; during the authentication process the direct access register is enabled, however the issue still remains: The Sciclient_procBootAuthAndStart() function returns with SystemP_FAILURE.
I also checked the Flash configuration as asked (Are you already running the flash at its maximum configurations like PHY enables, running at maximum clock, protocol 8D-8D-8D, etc.) and it's set up correctly.
As mentioned previously, I have tried to authenticate and boot the image by moving it to PSRAM, and the bootloader successfully booted it, so I can assume that the images and signatures/certificates are correct.
Could you please provide a solution for this?
Thanks, Mark