Part Number: MSPM0G1507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I was attempting to disable BSL in Non-Main Flash and then flash the code. However, after doing so, I'm unable to flash the program back with Jflash because JLINK is not connecting.
Additionally, I'm unable to debug in IAR.
Example code:
/*
* Copyright (c) 2021, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
#include "boot_config.h"
#include "ti_msp_dl_config.h"
/* clang-format off */
/* Base address of nonmain memory */
#define NONMAIN_BASE_ADDRESS (0x41C00000U)
/* Base address of the BCR configuration structure in nonmain memory */
#define BCR_USER_CFG_BASE_ADDRESS (0x41C00000U)
/* Base address of the BSL configuration structure in nonmain memory */
#define BSL_USER_CFG_BASE_ADDRESS (0x41C00100U)
/* Size in bytes of the BSL and BCR configuration structures */
#define BCR_CONFIG_SIZE_BYTES (96U)
#define BSL_CONFIG_SIZE_BYTES (88U)
/* The calculated CRC based on the default configuration values */
#define BCR_CFG_DEFAULT_CRC (0x1879dac3)
#define BSL_CFG_DEFAULT_CRC (0xf7df416)
/* clang-format on */
/* The default configuration of the BCR config struct */
BCR_Config gBCRConfig = {
.bcrConfigID = 0x1,
.debugAccess = BCR_CFG_DEBUG_ACCESS_EN,
.swdpMode = BCR_CFG_SWDP_EN,
.tifaMode = BCR_CFG_TIFA_EN,
.bslPinInvokeEnable = BCR_CFG_BSL_PIN_INVOKE_DIS,
.passwordDebugLock = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
.fastBootMode = BCR_CFG_FAST_BOOT_DIS,
.bootloaderMode = BCR_CFG_BOOTLOADER_MODE_DIS,
.massEraseMode = BCR_CFG_MASS_ERASE_EN,
.factoryResetMode = BCR_CFG_FACTORY_RESET_EN,
.passwordMassErase = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
.passwordFactoryReset = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
.staticWriteProtectionMainLow = CFG_DEFAULT_VALUE,
.staticWriteProtectionMainHigh = CFG_DEFAULT_VALUE,
.staticWriteProtectionNonMain = BCR_CFG_NON_MAIN_STATIC_PROT_DIS,
.secureBootMode = BCR_CFG_SECURE_BOOT_DIS,
.userSecureAppStartAddr = CFG_DEFAULT_VALUE,
.userSecureAppLength = CFG_DEFAULT_VALUE,
.userSecureAppCrc = CFG_DEFAULT_VALUE,
.userCfgCRC = 0x696128be,
};
/* The default configuration of the BSL config struct */
BSL_Config gBSLConfig = {
.configID = 0x1,
.interfacePins.UART_RXD_pad_num = DEF_UART_RXD_PAD,
.interfacePins.UART_RXD_PF_mux_sel = DEF_UART_RXD_MUX,
.interfacePins.UART_TXD_pad_num = DEF_UART_TXD_PAD,
.interfacePins.UART_TXD_PF_mux_sel = DEF_UART_TXD_MUX,
.interfacePins.I2C_SDA_pad_num = DEF_I2C_SDA_PAD,
.interfacePins.I2C_SDA_PF_mux_sel = DEF_I2C_SDA_MUX,
.interfacePins.I2C_SCL_pad_num = DEF_I2C_SCL_PAD,
.interfacePins.I2C_SCL_PF_mux_sel = DEF_I2C_SCL_MUX,
.pin.pinData0 = DEFAULT_BSL_PIN_INVOCATION_DATA0,
.pin.pinData1 = DEFAULT_BSL_PIN_INVOCATION_DATA1,
.memoryRead = BSL_CFG_MEMORY_READOUT_DISABLE,
.password = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
.pluginType = BSL_CFG_PLUGIN_TYPE_ANY,
.flashPluginEnable = BSL_CFG_PLUGIN_FLASH_NOT_EXIST,
.pluginSramSize = 0xff,
.pluginHook[0] = CFG_DEFAULT_VALUE,
.pluginHook[1] = CFG_DEFAULT_VALUE,
.pluginHook[2] = CFG_DEFAULT_VALUE,
.pluginHook[3] = CFG_DEFAULT_VALUE,
.BSLAlternateConfig = BSL_CFG_FLASH_BSL_NOT_EXIST,
.reserved = 0xFFFF,
.BSLAlternateAddr = CFG_DEFAULT_VALUE,
.appRev = (uint32_t *) CFG_DEFAULT_VALUE,
.securityAlert = BSL_CFG_SECURITY_IGNORE,
.i2cSlaveAddress = 0x48,
.userCfgCRC = 0xf7df416,
};
uint32_t calcUserConfigCRC(uint8_t *dataPointer, uint32_t size)
{
static uint32_t i;
uint32_t calculatedCRC;
DL_CRC_init(CRC, DL_CRC_32_POLYNOMIAL, DL_CRC_BIT_REVERSED,
DL_CRC_INPUT_ENDIANESS_LITTLE_ENDIAN, DL_CRC_OUTPUT_BYTESWAP_DISABLED);
/* Set the Seed value to reset the calculation */
DL_CRC_setSeed32(CRC, CRC_SEED);
for (i = (uint32_t) 0U; i < size; i++) {
DL_CRC_feedData8(CRC, dataPointer[i]);
}
calculatedCRC = DL_CRC_getResult32(CRC);
return calculatedCRC;
}
void DL_FlashCTL_executeClearStatus(FLASHCTL_Regs *flashctl)
{
/* Set COMMAND bit within CMDTYPE register to clear status*/
flashctl->GEN.CMDTYPE = DL_FLASHCTL_COMMAND_TYPE_CLEAR_STATUS;
/* Set bit to execute command */
flashctl->GEN.CMDEXEC = FLASHCTL_CMDEXEC_VAL_EXECUTE;
/* Wait for the clear status command to finish*/
while ((FLASHCTL->GEN.STATCMD & FLASHCTL_STATCMD_CMDINPROGRESS_MASK) ==
FLASHCTL_STATCMD_CMDINPROGRESS_STATINPROGRESS) {
;
}
}
int main(void)
{
SYSCFG_DL_init();
/*
* Calculate the CRC for the BCR and BSL configuration structs
* The CRC is 4 bytes in each struct, this should not be included in the calculation
*/
gBCRConfig.userCfgCRC = calcUserConfigCRC((uint8_t *) &gBCRConfig,
BCR_CONFIG_SIZE_BYTES - ((uint32_t) sizeof(gBCRConfig.userCfgCRC)));
gBSLConfig.userCfgCRC = calcUserConfigCRC((uint8_t *) &gBSLConfig,
BSL_CONFIG_SIZE_BYTES - ((uint32_t) sizeof(gBSLConfig.userCfgCRC)));
/* Clear STATCMD register, unprotect NONMAIN, and then erase NONMAIN memory */
DL_FlashCTL_executeClearStatus(FLASHCTL);
DL_FlashCTL_unprotectSector(
FLASHCTL, NONMAIN_BASE_ADDRESS, DL_FLASHCTL_REGION_SELECT_NONMAIN);
DL_FlashCTL_eraseMemoryFromRAM(
FLASHCTL, NONMAIN_BASE_ADDRESS, DL_FLASHCTL_COMMAND_SIZE_SECTOR);
/*
* Program the BCR config structure to NONMAIN memory.
* The BCR config struct has a size of 96 bytes, and 4 bytes are
* programmed at a time, resulting in 96 / 4 = 24 writes to Flash
*/
DL_FlashCTL_programMemoryBlockingFromRAM64WithECCGenerated(FLASHCTL,
BCR_USER_CFG_BASE_ADDRESS, (uint32_t *) &gBCRConfig,
(BCR_CONFIG_SIZE_BYTES / 4), DL_FLASHCTL_REGION_SELECT_NONMAIN);
/*
* Program the BSL config structure to NONMAIN memory.
* The BSL config struct has a size of 88 bytes, and 4 bytes are
* programmed at a time, resulting in 88 / 4 = 22 writes to Flash
*/
DL_FlashCTL_programMemoryBlockingFromRAM64WithECCGenerated(FLASHCTL,
BSL_USER_CFG_BASE_ADDRESS, (uint32_t *) &gBSLConfig,
(BSL_CONFIG_SIZE_BYTES / 4), DL_FLASHCTL_REGION_SELECT_NONMAIN);
/* After all writes, toggle LED */
while (1) {
DL_GPIO_togglePins(GPIO_LEDS_PORT, GPIO_LEDS_USER_LED_1_PIN);
delay_cycles(16000000);
}
}
Sysconfig:

Note: I have used the same parameters as code generated by Sysconfig tool.
I am using IAR and JFlash tool for my testing, so I am looking for related solutions.