This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1306: Programing MSPM0L1306SRHB from XDS110

Part Number: MSPM0L1306

Tool/software:

Hi TI, 

Can I program an MSPM0L1306SRHB from the XDS110 from (LPCC1311P3)?

I am trying to program it from an XDS110 but I get this error:

Is it possible to decrease the TCK speed? Would it help?

  • Hello,

    Yes, you can program any MSPM0 device with an XDS110, although I do not know what the LPCC1311P3 is. 

    Are you trying to program a black device or has it been programmed before?  DAP error can mean the debug interface is shutdown or possibly, that it's not seeing the target unit.  In the case that the debug port has been disabled, that's why it's suggesting trying to put the unit into BSL mode or factory resetting the device.    

    If this is a blank device and across a couple units, then it's most likely a physical connection/wiring issue. 

    Also, is the target MSPM0 being powered?  

    Thanks,

    JD

  • I assume an CC1311 Launchpad.