Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: AM2434, SYSCONFIG
Tool/software:
Hello, we are using a pair of DP83826 PHYs connected to an AM2434 for use in an EtherCAT subdevice (working OK).
We have connected the DP83826's LINK signals to PRG1_PRU0_GPO8 and PRG1_PRU1_GPO8 as per the documentation. I can see that SysConfig is correctly mapping them and I presume that the firmware is using them.
However, we have also been previously instructed by TI to connect the ACT and CRS signals into the GPO9 and GPO10 signals on PRU0 and PRU1 respectively.
They are not mentioned in the "PRU-ICSS EtherCAT Slave Firmware Data Sheet" nor in "How and Why to Use the DP83826 for EtherCAT® Applications" (for PRUs) and we particularly note that these signals are NOT mapped in SysConfig.
Given that we are short of IO, we are wondering if these connections are necessary.
Please kindly confirm whether or not ACT and CRS signals are necessary for AM243x EtherCAT subdevices (pointing to relevant documentation is always helpful).
Thanks, Steve