This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: No Pad

Part Number: MSPM0G3507

Tool/software:

how to reset when

 CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.
CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.
CS_DAP_0: GEL: Error while executing GEL_DAPInit_remoteFactoryReset(1): Connect failed
at GEL_Connect() [mspm0_cs_dap_init.gel:359]
at GEL_DAPInit_remoteSECAPCommand(0x020AU, autoReset) [mspm0_cs_dap_init.gel:323]
at GEL_DAPInit_remoteFactoryReset(1)