This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0714: TMS5700714APZQQ1 signal output is abnormal

Part Number: TMS570LS0714

Tool/software:

TMS5700714APZQQ1 signal output is abnormal, see PPT for detailsAnalysis report of TMS5700714APZQQ1.pptx

  • Hi,

    I want to check few questions:

    1. Is this board being custom board or TI-specific board?

    2. Is the part name on the controller is same for both the controllers? If possible, share a picture of them.

    3. Is the loaded application on the both the controller is same?

    --
    Thanks & regards,
    Jagadish.

  • 1.custom board
    2.Since coating has been done before, the marking information on the defective chip is not clear, but the batch information of the defective chip can be queried in the PPT.

    3.The loaded application on the both the controller is same.

  • 1.custom board
    2.Since coating has been done before, the marking information on the defective chip is not clear, but the batch information of the defective chip can be queried in the PPT.

    3.The loaded application on the both the controller is same.

  • Hi,

    My sincere apologies for the late response, i was stuck with other issues.

    Are you still stuck with this issue? If yes, then i can immediately start work on it and will try to provide an update.

    --
    Thanks & regards,
    Jagadish.

  • Hi,

    Is it possible to setup one live debugging session for this issue.

    This is required because, usually the controller GIO pins will not operate with any delay. If there is some issue with controller, then it will completely get failure but in our case, you are saying they are operating with some delay. So, i want to verify complete path on how you are operating pins.

    I will be available from 10AM to 7PM IST (Indian Standard Time), so based on your availability please set at meeting.

    --
    Thanks & regards,
    Jagadish.

  • Now we have a lot of bad problems with RELAY moved intermittently, please pay attention to this problem first.
    As for the problem of RELAY moved intermittently, I analyzed it as follows: I connected one end of the probe of the oscilloscope to the RELAY_SET and RELAY_RESET signals of the chip, grounded the other end, and sent instructions for realy to move at this time. It was found that the signal sent by the U1 chip was intermittent, and the details of the picture were shown in PPT.

    There was something wrong with my translation in the PPT before, now I have changed it, you can check it in the attachmentAnalysis report of TMS5700714APZQQ1(1111).pptx

  • Is it possible to have one live debugging session?

    I will be available from 10AM to 7PM IST (Indian Standard Time), so based on your availability please set at meeting.