Part Number: MSPM0G3507
Tool/software:
Dear,
I'm sending consequently 3 messages to MCAN using the following code.
When I step through it, all 3 messages appear on the CAN bus.
When is it running (short time between calling this routing), only one meassage is appearing on the CAN bus.
I tried several things like checking if the msg was added (tested using DL_MCAN_TXBufAddReq return value == 0).
Code:
bool canTxFifo(union MESSAGE *txMessage)
{
DL_MCAN_TxEventFIFOStatus fifoStatus;
bool ret;
DL_MCAN_getTxEventFIFOStatus(MCAN0_INST, &fifoStatus);
if (!fifoStatus.fifoFull)
{
txMsg.id = txMessage->can.id << 18U;
for (uint32_t i = 0; i < 8; i++) txMsg.data[i] = txMessage->can.data[i];
DL_MCAN_writeMsgRam(MCAN0_INST, DL_MCAN_MEM_TYPE_FIFO, 0, &txMsg);
DL_MCAN_TXBufAddReq(MCAN0_INST, 0);
return true;
}
else
return false;
}
Many thanks for help!