Part Number: AM2434
Tool/software:
Hi there , how many motors can am2434 control with EnDat?
best, Jinlong
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2434
Tool/software:
Hi there , how many motors can am2434 control with EnDat?
best, Jinlong
Hi
It depends on other system requirements.
Technically, we can do 12x EnDat interfaces with 2x PRI-ICSSG from 1 AM243x. But let's say if you need one Industrial Communication interface (like EtherCAT, Profinet, EtherNet/IP, etc), it will take up one PRU-ICSSG. If you also need current sense using SDFM, 0.5x PRU-ICSSG is needed for 9x SDFM channels. In this case, you can implement 3-axis motor control using 1x AM243x, where 1x PRU-ICSSG does industrial communication and other PRU-ICSSG does 3x EnDat and 9x SDFM. Also we only have 9x SoC EPWMs on chip. But we also have additional PWMs which can be implemented with ICSS PWM.
Please refer to AM243x Motor Control SDK: Introduction for more details. Also, we have a 2-axis reference design :TIDEP-01032 EtherCAT-Connected Single-Chip Dual-Servo Motor Drive Reference Design
Regards
Dhaval
Thanks. Can you image any possibility to run 4 motors with a single AM2434 with EnDat and SDFM for each and every motor, where one PRU-ICSSG is taken by one industrial communication interface?
Hi
It is difficult to do 4 encoders and SDFM with 1x PRU-ICSSG. If you use ADC for current sense instead of SDFM, we can use 1x PRU-ICSSG for 4x EnDat as we do not need to do SDFM using PRU-ICSSG.
Regards
Dhaval
Thanks. The number of motors is clarified.
Another question, we do not use EnDat encoder. Instead, we use rotary encoder. Do you have an example project for one or two motors?
Hi
What is the interface for this rotary encoder?
https://software-dl.ti.com/processor-industrial-sw/esd/motor_control_sdk/am243x/09_02_00_09/docs/api_guide_am243x/index.html has details on supported interfaces for encoders.
Regards
Dhaval
Not EnDat encoder or other encoders listed on your web page.
We will use eqep: channel a, channel b, and channel i. Each rotation will have four square signal; phase between channel A and channel B indicates direction of rotation.
Hi Jinlong, there is an EQEP Capture example in our MCU+SDK
AM243x MCU+ SDK: EQEP Capture. for this example EQEP is signals are generated using GPIO toggling. Example check EQEP_A and EQEP_B signals clockwise and counterclockwise
Few more details: AM243x MCU+ SDK: EQEP
APIs: AM243x MCU+ SDK: APIs for EQEP
thank you,
Paula