This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM263P: AM263P + DP83822 MII loopback

Part Number: LP-AM263P
Other Parts Discussed in Thread: DP83822I

Tool/software:

Hi,

 

  We are facing issue with the Ethernet communication in Dp83822i PHY .

Have tried Multiple settings in the PHY registers and have mentioned the status below.

 

Controller : AM263px

 

Controller To PHY:

 

   1) MDIO Pins - Read/Write PHY Registers - OK

   2) PHY Address detecting                - OK

   3) When Loop back Mode Enabled , Loopback function is not working (Internal Transmit and receive )      - NOT OK

 

PHY TO PC:

 

   1) Once, When Loopback Mode Enabled and an ethernet cable connected between PHY to PC, there occurs a packet transmission between

       PC to PHY. Which is not the intended behaviour.   - NOT OK     

   2) In normal mode (when Loopback mode is disabled )- Transmit/Receive not working (between PC to PHY)  - NOT OK        

   3) Auto Negotiation (100/ 10mbps half-duplex and 10 mbps Full Duplex) - working (From read status of 0x0005 Register),

      but there is no communication between PHY to PC or vice versa.  - NOT OK

   4) 100Mbps Full duplex Auto negotiation is not Working (its auto negotiating to 100mbps Half duplex only)  - NOT OK