Part Number: TM4C1294NCPDT
Tool/software:
Hello, i am trying to run Enet_TCP_ECHO SERVER example provided in examples with tivaware.
When i first run the program i realized it didn't work, because it got stuck reading the mac address which i have not programmed in.
So i removed the mac address reading part and added it manually.
pui8MACArray[0] = 0x70; pui8MACArray[1] = 0xFF; pui8MACArray[2] = 0x76; pui8MACArray[3] = 0x1F; pui8MACArray[4] = 0x83; pui8MACArray[5] = 0x79;
After this change the pf4 led started blinking and pn0,pf0 was always on but i could not connect my tcp server with putty
i have entered 168.168.1.100 and port 23 in putty with telnet selected.
But it kept refusing the connection.
I looked the program and i saw it was waiting for me to give ip address, so i have changed to use static address.
#define IPADDR(a,b,c,d) ((uint32_t)((a) | ((b) << 8) | ((c) << 16) | ((d) << 24))) #define STATIC_IP_ADDRESS IPADDR(168,168,1,100) #define NETMASK IPADDR(255,255,255,0) #define GATEWAY IPADDR(168,168,1,1) lwIPInit(g_ui32SysClock, pui8MACArray, STATIC_IP_ADDRESS, NETMASK, GATEWAY, IPADDR_USE_STATIC);
i use the IPADDR function to change the values into little endian also changed values in lwipopts.h ;
#define LWIP_AUTOIP 0
#define LWIP_DHCP 0
But currently it is still refusing connection.