This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
3) what is the behavior when VDD goes above from 1.62v to ~(3.3v - 3.9v)? As per waveform it should be in running state. but as per my observation still MCU is in reset state.
Are the contents of SRAM guaranteed to be valid when VDD is in between 1.62 to 3.9v?
Hello Sourabh,
1). After VDD goes above 1.62 V, and then Vcore will start to rise to about 1.35 V. After that it will start to run the boot code in ROM and then to run the application code in Flash. Please check your Vcore voltage and the Cap value near Vcore and VDD;
2). Please check the voltage on NRST pin;
3). Our recommend voltage on VDD which can make MCU work normally is 1.62 ~ 3.6 V, why you need to add to 3.9 V?
Best Regards,
Janz Bai
1)
i) Cap near Vcore is 470nF
ii) Cap near VDD is 10uF and 100nF in parallel
2) NRST pin is low after 1.62v
3) In the voltage range 1.62 ~ 3.6 V MCU still in reset state. after ~3.9v to 4v MCU is getting ON.
voltage on NRST pin
Hello Sourabh,
1). What is the meaning of "NRST pin is low after 1.62 v"? It means that NRST will be low after VDD raises to 1.62 V, or it means that NRST voltage is lower than 1.62 V?
2). How do you judge that MCU is in reset state, observing something?
3). Our recommend voltage on VDD which can make MCU work normally is 1.62 ~ 3.6 V. The goal of rising VDD to 4.0 is just for tests or it is the requirement of your factual application? If you keep the VDD voltage at 3.3 V, the MCU will always in reset state?
4). What is the voltage on Vcore in your test process?
5). In fact, if NRST is high voltage and Vcore voltage is correct, and Cap near VDD and Vcore is correct, MCU must work normally at 3.3 V. Do you have MSPM0L1306 LaunchPad, you can download example code in SDK to M0 and check whether it can work normally.
Please help to confirm this points.
Best Regards,
Janz Bai
1) NRST pin is low low after VDD raises to 1.62 V
2) Togging GPIO pin to judge that MCU is in reset state or not.
if MCU is in reset state GPIO pin will not toggle after reset GPIO pin will toggle.
3) Yes, when VDD voltage at 3.3 V MCU is in reset state.
4) I will check the voltage
5) I don't have MSPM0L1306 LaunchPad. I am testing on custom board, which has LIN Transceiver connected to MCU
Hello Sourabh,
Why NRST is low? If it's pulled down to low, it will make MCU in reset state. Please check why the NRST is low after VDD raises to 1.62 V, and check the NRST voltage when the VDD is 3.9 V ~ 4 V. In fact, our MCU VDD can't set to 4 V because it may cause MCU work abnormally, but I want to know the NRST voltage when VDD is over 3.9 V.
So if you keep VDD 3.3 V forever, MCU will always in reset state, and GPIO will never toggle, right?
In fact, I think maybe MCU has been broken when you raise VDD over 3.6V for many times.
Best Regards,
Janz Bai