Part Number: TMS570LC4357
Tool/software:
Hello,
I think i have identified a discrepancy in the documentation of the MSTGENA field descriptions for the Memory Self-Test Controller Global Enable Key. This needs to be reviewed and corrected to align with the intended functionality and ensure clarity for developers.
SPNU563A–March 2018
Table 2-39. Memory Self-Test Global Control Register (MSTGCR) Field Descriptions
Discrepancy Details:
-
Current Documentation:
- The documentation specifies:
Ah Memory self-test controller is enabled Others Memory self-test controller is disabled. - Note included:
Note: It is recommended that a value of Ah be used to disable the memory self-test controller. This value will give maximum protec...
- The documentation specifies:
-
Issue:
- There is a contradiction in the documentation regarding the value 'Ah'. Initially, it states that the value 'Ah' enables the memory self-test controller. However, the note later suggests that the value 'Ah' should be used to disable the memory self-test controller.
- The end of the note is cut off, making the recommendation incomplete