Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4: When using ccs theia, a compilation problem was encountered. The assembly code of the .s file reported errors

Part Number: AM263P4

Tool/software:

    This is a screenshot of a compilation error. It appears that the compiler cannot parse the.s file correctly. But these files in another project is not compiling errors, and can run normally, is there any compiler options not configured correctly

  • You show screenshots from the Problems view of the Panel.  That lacks detail I need to see.  Capture the contents of the Output view from the Panel not with a screenshot, but in a text file.  While your mouse is active in the Output view, right click and select Copy All.  Paste into a text file.  Be sure this file uses the file extension .txt.  Attach it to your next post.  

    The first error diagnostic indicates there is a problem with line 1 of the assembly source file.  Please attach the assembly source file.  Or at least show this first line.  Please copy and paste the text, and do not use a screenshot.

    Thanks and regards,

    -George