Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI Experts,
Customer is working on AM2432 SDK9.2.
Environment: They are using AM24x LaunchPad Board.
They are currently implementing the firewall applications on Main R5fss0-0 & Main R5fss1-0 respectively.
With the same firewall configuration below for UART0 instance, they could run normally on Main R5fss0-0, but will fail on Main R5fss1-0.

When it fails on Main R5fss1-0, the result is shown below.

Apart from this, customer also tried the same configurations for GPIO instance firewall, and the result is the same, run normally on Main R5fss0-0, but will fail on Main R5fss1-0
Hence, there are two questions from customer below.
1: Is there some configurations setup not correct which may cause this problem?
2: If the configurations are correct, then does that mean only Main R5fss0-0 core could do the firewall, and Main R5fss1-0 is not possible? Is this result the same that apply to AM2432 ALX?
Many Thanks,
Kevin