Part Number: AM2434
Tool/software:
Hi,
This is additional questions to the original thread.
Based on the answer provided in the last post (below), the customer checked JEDEC (JESD79-4).
> all these values should be taken from the JEDEC spec, as the SoC interface will be compatible with those specs.
But there is no values for DDR controller side to below parameters.
tDASS : time between CLK output to DQS output
tIS, tIH : time between CLK output to ADR/CMD output
tDS, tDH : time between DQS output to DQ/DM output
How AM243x was validated to meet JEDEC spec?
If simulation was done, what values were used delay values for each timing?
Thanks and regards,
Koichiro Tashiro