Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hello Team
I am testing on AM243x EVM board.
I use DFU boot loader to initialize the Soc and load the firmware to RAM. And then to communicate with Soc USB through NI VISA.
I have installed the NI VISA Tool and the Soc's DFU USB port can be recognized in Device Manager.
But after execution of DFU boot loader, the USB control disappear in Device Manager, NI VISA cannot talk to USB either.
I need to know if there is solution to keep the USB control after the DFU boot loader without power cycle or warm reset the Soc.
Thanks.
Thanks & Best regards
Hao (Wang hao)