This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
My customer use IAR 9.50.2 to develop M0G3507 FW. While debugging in low power mode, they meet below error.
They refer to below links. It needs to have armXDS.dll . Please instruct where to get this file (armXDS.dll) ?
https://dev.ti.com/tirex/explore/node?node=A__ANSP7A0xhIl-tGV4vBLoMg__MSPM0-SDK__a3PaaoK__LATEST
Thank you.
Hi Jerry,
I think the armXDS.dll can be found in a latest version of IAR like v9.60.2. However, I checked with the team. No one has installed this new version on their PC. So, it would need to check with ARM to ask if they can send it to your customer.
Best regards,
Cash Hao
Hi Poca,
I check the latest version IAR ARM is 9.60.3. Would you check the latest IAR version ?
Hi Cash and Jerry,
So, it would need to check with ARM to ask if they can send it to your customer.
The latest IAR version is v9.50.2 or v9.50.4. They don't have the 9.60.3, could we send the v9.60.2/v9.60.3 IAR ARM to the customer?
Without this, they can't operate the debug tool normally.
Hi,
I installed v9.60.3 on my PC. And find this .dll file.
Please use it and try if it can work on your side. Change the .txt to .dll on your side.
Best regards,
Cash Hao
Please use it and try if it can work on your side.
Do you mean with "IAR v9.60.3 and its armXDS.dll", M0G can enter low power mode under debug ?
My customer try with "IAR 9.50.2 + armXDS.dll from 9.60.3" and M0G cannot enter low power mode under debug. They have the authorized license of IAR 9.50.2 and follow the instructive steps from E2E
Hi Jerry,
Yes, according to below information. Using IAR v9.50.2 + armXDS.dll and the .dmac file from the latest SDK should support M0 MCU enter low power mode while debugging.
Best regards,
Cash Hao
Hi team,
My customer follow up above instructions. But they meet below error. Please help clarify. Thank you.
Hi Jerry,
If it does not work. Then it will requires customer to update their IAR version to 9.60.2 to avoid that issue. Or use CCS to debug.
Best regards,
Cash Hao