Part Number: TMDSCNCD263P
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
I am getting an error using the AM263P Control Card and Uniflash programmer.
It is strange it says 0 of 32752 when the file size is 219.39 KB!
Board: AM263P Control Card
Uniflash: 8.7.0 and 9.0.0, same error both versions
SDK: 10.1.0.31
SBL Image: sbl_ospi.release.tiimage
OS on host computer: Windows10
SOP3,SOP2,SOP1,SOP0
1 0 1 1 = DevBoot
0 0 1 1 = OSPI(8S), 50MHz
With CCS I can run "ospi_flash_diag_am263px-cc_r5fss0-0_nortos_ti-arm-clang" using JTAG and all the OSPI flash diagnostics PASS OK.