This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXRM46HDK: FEE not Initializing



Tool/software:

i am trying to use the FEE api and i am not getting through initialization 

this code is the first called from my main()

uint16_t Status;
TI_Fee_Init();
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
if (Status != IDLE){
TI_Fee_ErrorCodeType ec = TI_FeeErrorCode(0);
TI_Fee_ErrorRecovery(ec,0 );

}
}
while(Status!= IDLE);

if never gets out of the do/while loop and always has  "Error_SetupStateMachine" as the error code.

Setupflash look like this

void setupFlash(void)
{

/* USER CODE BEGIN (6) */
/* USER CODE END */

/** - Setup flash read mode, address wait states and data wait states */
flashWREG->FRDCNTL = 0x00000000U
| (uint32)((uint32)2U << 8U)
| (uint32)((uint32)0U << 4U)
| 1U;

/** - Setup flash access wait states for bank 7 */
FSM_WR_ENA_HL = 0x5U;
EEPROM_CONFIG_HL = 0x00000002U
| (uint32)((uint32)3U << 16U) ;

/* USER CODE BEGIN (7) */
/* USER CODE END */

/** - Disable write access to flash state machine registers */
FSM_WR_ENA_HL = 0xAU;

/** - Setup flash bank power modes */
flashWREG->FBFALLBACK = 0x00000000U
| (uint32)((uint32)SYS_ACTIVE << 14U) /* BANK 7 */
| (uint32)((uint32)SYS_ACTIVE << 2U) /* BANK 1 */
| (uint32)((uint32)SYS_ACTIVE << 0U); /* BANK 0 */

/* USER CODE BEGIN (8) */
/* USER CODE END */

}

i have tried changing to svc mode before the calls and still getting the same.