Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
Hi,
I am working on an application with a bootloader. Without using the FEE Driver, the bootloader and application code work fine without any errors. When I add the FEE Driver and use it without the application code, it also works without issues. There is no problem up to this point. However, when I use the bootloader and my application with the FEE Driver, it causes a prefetch error.
When I debugged the code, after some trials, I realized that the TI_Fee_WriteAsync function causes the prefetch error. When I comment out this function in the application code, everything works fine. I am sharing the .cmd files for the bootloader and application code. Are there any suggestions to solve this problem? Thanks.
Bootloader .cmd file:
/* */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Linker Settings */
--retain="*(.intvecs)"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00010000 length=0x00000020
FLASH0 (RX) : origin=0x00010020 length=0x0012FFE0
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0002EB00
/* USER CODE BEGIN (2) */
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI:
{
.\source\bl_flash.obj(.text)
--library=F021_API_CortexR4_BE.lib(.text)
}palign=8 load=FLASH0, run=RAM, LOAD_START(apiLoadStart), RUN_START(apiRunStart), SIZE(apiLoadSize)
.text : {} > FLASH0
.const : {} > FLASH0
.cinit : {} > FLASH0
.pinit : {} > FLASH0
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
FEE_TEXT_SECTION : {} > FLASH0
FEE_CONST_SECTION : {} > FLASH0
FEE_DATA_SECTION : {} > RAM
/* USER CODE BEGIN (4) */
/* USER CODE END */
}
/* USER CODE BEGIN (5) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Misc */
/* USER CODE BEGIN (6) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
Application cmd file:
/* */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Linker Settings */
--retain="*(.intvecs)"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0013FFE0 // OD length=0x0013FFE0 -->> length=0x0000FFFF
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0002EB00
/* USER CODE BEGIN (2) */
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI:
{
.\fapi\\source\Fapi_UserDefinedFunctions.obj(.text)
.\source\bl_flash.obj(.text)
--library=F021_API_CortexR4_BE.lib(.text)
}palign=8 load=FLASH0, run=RAM, LOAD_START(apiLoadStart), RUN_START(apiRunStart), SIZE(apiLoadSize)
.text : {} > FLASH0
.const : {} > FLASH0
.cinit : {} > FLASH0
.pinit : {} > FLASH0
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
/* USER CODE BEGIN (4) */
/* USER CODE END */
}
/* USER CODE BEGIN (5) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Misc */
/* USER CODE BEGIN (6) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/