Part Number: RM46L852
Tool/software:
I have been working for RM46 bootloader using CAN
let me get directly into point that After copying Flash API to RAM the functions like Fapi_initializeAPI() AND Fapi_initializeFlashBanks() are not getting executed properly and not running do i need to add anything more in the liker command .
i attached linker command below
your suggestions are highly appreciated.
Thank you
--retain="*(.intvecs)"
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH_API (RX) : origin=0x00000020 length=0x000024E0
FLASH0 (RX) : origin=0x00002500 length=0x002FEB00 //LS31x and RM48 Flash size is 0x300000
SRAM (RW) : origin=0x08002000 length=0x0002D000
STACK (RW) : origin=0x08000000 length=0x00002000
}
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI :
{
..\Release\F021_API\Fapi_UserDefinedFunctions.obj (.text)
..\Release\bl_flash.obj (.text)
--library= F021_API_CortexR4_LE_V3D16.lib < FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.SetActiveBank.obj
FlashStateMachine.InitializeFlashBanks.obj
FlashStateMachine.EnableMainSectors.obj
FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.ScaleFclk.obj
Init.obj
Utilities.CalculateEcc.obj
Utilities.WaitDelay.obj
Utilities.CalculateFletcher.obj
Read.MarginByByte.obj
Read.Common.obj
Read.FlushPipeline.obj
Read.WdService.obj
Async.WithAddress.obj
Program.obj > (.text)
} load = FLASH_API, run = SRAM, LOAD_START(api_load), RUN_START(api_run), SIZE(api_size)
.text > FLASH0
.const > FLASH0
.cinit > FLASH0
.pinit > FLASH0
.data > SRAM
.bss > SRAM
}