Part Number: TM4C129EKCPDT
Other Parts Discussed in Thread: ARM-CGT
Tool/software:
Hi,
I would be very grateful for confirmation that it is possible to use TI ARM Clang for TM4C devices.
My concern is the final answer to the following post:
TM4C123GH6PZ: driverlib and ti-cgt-armllvm_4.0.1.LTS wchar_t incompatibility
Here is the part that concerns me:
TM4C Driverlib is not compatible with Clang compiler. Please use TI Arm compiler only for TM4C device. You can download the latest TI Arm compiler from https://www.ti.com/tool/ARM-CGT.
I am not sure how to understand the sentence above.
Please confirm: can I compile my application code with TI ARM Clang (ARM-CGT-CLANG) and link it with Driverlib compiled with TI ARM compiler (ARM-CGT)?
The TI Arm Clang Compiler Tools User's Guide v4.0 lists Cortex-M4 as one of the supported processors, other discussions like TM4C1290NCPDT: TI ARM Clang Migration and Tiva Bootloader issue suggest that it is possible to use TI ARM Clang for TM4C devices.
I understand that the source code of the TM4C Driverlib is not compatible with TI ARM Clang, so the Driverlib has to be compiled using standard TI ARM compiler (ARM-CGT). I also understand that the resulting linker warnings about wchar16_t are essentially harmless. But can I use Clang to compile my code and use Driverlib compiled by standard TI ARM compiler?
I am asking because I... think I might have found a bug in ARM-CGT and switching to TI ARM Clang solves the problem, which is very important for me. That's why I'd be particularly grateful for any information.
Best regards,
Kuba