This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC33XX-SOFTWARE: AM243x LaunchPad (AM243x-LP) and the CC33xx Lx Base Board - issue in Serial monitor output

Part Number: CC33XX-SOFTWARE

Tool/software:

Hi,

 I have flashed program_application_and_wifi_fw.cfg file to the Flash memory using the Command prompt while device is in UART boot mode. I got the expected output of flashing. I have attached the image of the output.

Then, changed the boot mode to QSPI, then powered on and monitored the output in serial monitor. I'm getting 'some test has failed'. I have attached my setup and output image below. What could be the issue, the issue is in hardware or Software? Kindly give some guidance?

I tried to flash only_wifi_fw.cfg file. I'm getting the same output.