Part Number: TMS570LC4357
Tool/software:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 12.7.0.00105)
Hello,
I am facing an issue with the LC43x development kit. when powered ON using the USB interface, the D12 LED turns on. But when I try to flash it , it fails with the above error.
Also while trying to flash, none of the LEDs D52, 53. 54 or 55 tend to glow.
I need some help in solving this issue.
Thank you !