Other Parts Discussed in Thread: ISO1042-Q1
Tool/software:
Hi,
We are using AM2634 with custom designed hardware which contains CAN Transceiver "ISO1042-Q1 " along with CCS Version 12.7.0.00007 and XDS110 Debugger.
We are Facing an issue with CAN when we are communicating with four nodes using CAN FD mode of which 3 are transmitting at distinct time intervals and one node is always receiving. And after some time, we are getting the receiving interrupt as Message stored to Dedicated Rx Buffer but in NDAT1 and NDAT2 registers no bit is set. we are only facing this issue when 4 nodes have been configured of which 3 are transmitting at different time intervals and one node is only recieving.