This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: I am trying to generate sci receive interrupt using Vim module of TMS570LC4357 but unable to generate receive interrupt. The main.c file i have attach below please help me out to generate interrupt.

Part Number: TMS570LC4357

Tool/software:

/** @file HL_sys_main.c 
*   @brief Application main file
*   @date 11-Dec-2018
*   @version 04.07.01
*
*   This file contains an empty main function,
*   which can be used for the application.
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com  
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* USER CODE END */

/* Include Files */

#include "HL_sys_common.h"
#include "HL_system.h"

/* USER CODE BEGIN (1) */
#include "HL_sci.h"
#include "HL_sys_core.h"
#include "HL_esm.h"
#include "HL_sys_vim.h"
#include "string.h"

#define UART sciREG3  // Use SCI3 for communication
void sciNotification(sciBASE_t *sci, uint32 flags);
void check_VIM_interrupts(void);
void check_VIM_dispatch(void);
void sci3_init();
void sci_send_string(sciBASE_t *sci, char *text, uint32 length);
uint8 message[] = "Hello, World!\r\n";

volatile uint8 received_data = 0;
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */

/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */
    systemInit();
    sciInit();  // Initialize SCI (Configured in HALCoGen)
//    sci3_init();  // Initialize SCI3 and enable interrupts
    _enable_interrupt_(); // Enable Global Interrupts

    //     Enable RX Interrupt for SCI3
        sciEnableNotification(sciREG3, SCI_RX_INT);

        ////     Enable SCI3 High Interrupt in VIM (SCI3 High is on Channel 64)
            vimEnableInterrupt(64, SYS_IRQ);
        //

        //Enable IRQ
            _enable_IRQ_interrupt_();

       sciSend(sciREG3, sizeof(message) - 1, message);  // Send message via SCI3

    volatile int i=0;
       while(1) {
//           sciSendByte(sciREG3, 'A');  // Send 'A' via SCI3
//           for ( i = 0; i < 1000000; i++);  // Small delay
//           sciSend(sciREG3, sizeof(message) - 1, message);  // Send message via SCI3
//                 for (i = 0; i < 5000000; i++);  // Small delay
//           if (sciIsRxReady(sciREG3)) {  // Check if data is available
//                       received_data = sciReceiveByte(sciREG3);
//                       sciSendByte(sciREG3, received_data);  // Echo back
//                   }
       }

       return 0;

/* USER CODE END */

//    return 0;
}


/* USER CODE BEGIN (4) */
//void sci3_init() {
//    sciInit();  // HALCoGen generated function
//
////     Enable RX Interrupt for SCI3
//    sciEnableNotification(sciREG3, SCI_RX_INT);
//
////     Enable SCI3 High Interrupt in VIM (SCI3 High is on Channel 64)
//    vimEnableInterrupt(64, SYS_IRQ);
//
////     Enable IRQ
//    _enable_IRQ_interrupt_();
//}

// SCI3 Interrupt Service Routine (ISR)
void sciNotification(sciBASE_t *sci, uint32 flags) {
    if (sci == sciREG3 && (flags & SCI_RX_INT)) {
        received_data = sciReceiveByte(sci);  // Read received byte
        sciSendByte(sci, received_data);      // Echo received byte
    }
}

/* USER CODE END */