Part Number: LP-AM243
Tool/software:
Hi,
If the RBL fails to load an image (SBL) with 0x0, an image (SBL) with 0x400000 will be loaded.
I would like to load a backup (read-only) image file into OSPI and boot that image if the SBL fails to authenticate the image file.
Q1) Is it possible, for example, to write an image file to the eFuse area? If so, can it be written with the OTP Keywriter?
Q2) If writing to eFuse is not possible, is there any other way?
Regards,
Yukinobu