This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01032: HDSL Safe Position Interrupt

Part Number: TIDEP-01032

Tool/software:

Dear Ti Experts

Which interrupt should I use to get data Safe Position Data in V-Frame. Is this interrupt  triggered exclusively for Safe Position Update.

Thank you

Alan I

  • Hi Alan,

    For Safe Position Data (VPOS), PRU0_ARM_IRQ1 is the interrupt associated with it. Also, please refer below info for the interrupt mapping:
    PRU0_ARM_IRQ4: EVENT_S

    PRU0_ARM_IRQ3/5: H-Frame

    PRU0_ARM_IRQ2: VPOS2 (Safe Position 2)

    PRU0_ARM_IRQ1: VPOS (Safe Position)

    PRU0_ARM_IRQ: EVENT_L 

    Let me know if you have any further questions.

    Best Regards,

    Rajul

  • Thank you for the reply

    I am running SYNC MODE , ES=4

    SYNC Period = 18750

    Sync Calculation is giving the following

    ********************************************************************
    SYNC MODE: period = 18751
    SYNC MODE: ES = 4
    SYNC MODE: counter = 269
    SYNC MODE: wait_before_start = 9349
    SYNC MODE: bottom_up_cycles = 18748
    SYNC MODE: extra_size = 5
    SYNC MODE: temp_gRest = 7
    SYNC MODE: extra_edge = 254
    SYNC MODE: num_of_stuffing = 5
    SYNC MODE: extra_size_remainder = 1
    SYNC MODE: stuffing_remainder = 2
    ********************************************************************

    1) SYNC MODE period is :18751  instead of 18750

    And the VPOS2 interrupt is drifting against reference interrupt with period of 18750.

    2) Changed the setting to 

    ES=4 

    SYNC Period = 18749

    ********************************************************************
    SYNC MODE: period = 18750
    SYNC MODE: ES = 4
    SYNC MODE: counter = 278
    SYNC MODE: wait_before_start = 9349
    SYNC MODE: bottom_up_cycles = 18748
    SYNC MODE: extra_size = 5
    SYNC MODE: temp_gRest = 7
    SYNC MODE: extra_edge = 254
    SYNC MODE: num_of_stuffing = 5
    SYNC MODE: extra_size_remainder = 1
    SYNC MODE: stuffing_remainder = 2
    ********************************************************************

    VPOS2 interrupt seems more stable against reference interrupt

    Is this expected?

    Alan I

  • Hi

    How are you giving SYNC pulse here? Are you using SDK example only?


    And the VPOS2 interrupt is drifting against reference interrupt with period of 18750.

    What do you mean by reference interrupt here?

    Regards

    Dhaval


  • Hi Alan,

    These are the calculations explained for sync mode for ES=1 and PRU frequency =225MHz. While capturing period of sync, there is 1 cycle latching error expected when taking sync input from internal IEP pulse. Have you tried SYNC Mode with providing external Sync pulse? 

    Best Regards,

    Rajul