Part Number: MSPM0L1306
Tool/software:
Hello,
So I've been looking at the IO state on reset again, and I think there's a case that isn't clear in the TRM what the state of the IO will be.
The case is if you're using the nRST signal to reset the MCU you can either generate a POR where it is clear in the TRM that the IO pins will be Hi-Z, but if you assert nRST for less than 1 second you go into BOOTRST which doesn't indicate if the IOs are reset to Hi-Z? It just says that you run the BCR and eventually end up in RUN. But what happens when the MCU has configured IO and then gets reset?
Is Hi-Z the default unless latched by the SHUTDOWN mode?
Munan