Part Number: TMDS243EVM
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG, AM2434, AM2432
Tool/software:
Hi Ti Expert,
I have an our own designed board whose main IC is AM2432BSEFHIALVR.
The following related part of our schematic is no difference from TMDS243EVM's.
I accorded to the following link to load the SBL to my board for the first time.
I tried Flash SOC Initialization Binary and SOC Initialization Using SD BOOT.
For Flash SOC Initialization Binary, on Uart mode, it stuck here.
PS C:\ti\mcu_plus_sdk_am243x_09_02_01_05\tools\boot> python uart_uniflash.py -p COM13 --cfg=sbl_prebuilt/am243x-evm/default_sbl_null.cfg
Parsing config file ...
Parsing config file ... SUCCESS. Found 2 command(s) !!!
Executing command 1 of 2 ...
Found flash writer ... sending sbl_prebuilt/am243x-evm/sbl_uart_uniflash.release.hs_fs.tiimage
Sent flashwriter sbl_prebuilt/am243x-evm/sbl_uart_uniflash.release.hs_fs.tiimage of size 324798 bytes in 33.53s.
Executing command 2 of 2 ...
Command arguments : --file=sbl_prebuilt/am243x-evm/sbl_null.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
Sending sbl_prebuilt/am243x-evm/sbl_null.release.hs_fs.tiimage: 0%| | 0/292638 [00:00<?, ?bytes/s]s
For SOC Initialization Using SD BOOT there was nothing printed through Uart.
Then I tried UniFlash tool, there was also an error and failed. (I selected the right chip, and there showing: MAIN_Cortex_R5_0_0 Disconnected: Running Free the R5)
Error: File: C:/Users/cfue07770/workspace_v12/sbl_null.debug.hs_fs.tiimage: Load failed.
[ERROR] MAIN_Cortex_R5_0_0: File Loader: Memory write failed: Unable to read algorithm file "C:\ti\uniflash_8.7.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\..\..\sitara_mcu\flasher\"
I have no idea what to do next, would you please guide me to load SBL and Application Image to my board for the first time?
By the way I found the following picture from api_guide_am243x/EVM_SETUP_PAGE is not match to the Technical Reference Manual.
It seems like they are Opposite. TRM shows: OSPI B3:B6 1000, while the EVM_SETUP_PAGE shows B3:B6 0111.
Am I misinterpreting or there is sth wrong?

BR,
Chunyang