Part Number: TMS570LC4357
Tool/software:
Hello,
Normally I can use TI FEE write operation without a problem. But whenever I change something in the code that is unrelated to the FEE code the write function causes a prefetch abort at (0xF0200578). I realized that it works fine if the loaded code size (.text) is some particular value lets say 0x455b0. And in the not-working code the loaded code size is less than it for example 0x37e84. Even though a small change in the code is applied, the loaded code in the debugger changes like 49kB.
When I look at the linker map file. I realized that there is an extra line in the segment allocation map between .text and .const lines in the not working code. So the FEE_TEXT_SECTION and FEE_CONST_SECTION look like not loaded. I could not share screenshots because of the network.
I am not using any OS. I am trying to write to Bank-7.
I would be very grateful if you can help me with this issue.
Thanks,
Best regards