This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0232: Remove zero fill from binary file generated by CC studio

Part Number: TMS570LS0232

Tool/software:

Is there an option to remove the 0x00 fill in the binary file when building with CC?

 Our flash section is only partially filed, but it's filling the rest of the section with zeroes, which massively increases the flashing time.


         name            origin    length      used     unused   attr    fill
----------------------  --------  ---------  --------  --------  ----  --------

  FLASH0                00021500   0013eb00  000c69f2  0007810e  R  X

Is there a way to prevent CC to fill the memory with zeroes or do I have to make my FLASH0 section smaller?

Thanks,

Quentin.