Part Number: AM2632-Q1
Other Parts Discussed in Thread: AM2632
Tool/software:
Hello! I have a question and would like to ask you for an answer. Fault phenomenon: The PCBA has been re-soldered but the software has not been burned in yet. After using 12V power supply, the current is approximately 100mA. The temperature of the AM2632 MCU chip is too high (at room temperature, the temperature exceeds 60℃). Our question is: 1. When the external FLASH of AM2632 is not programmed, does the MCU already have its own program inside? 2. Why is the temperature of the MCU so high? Under what circumstances would this fault phenomenon occur? Currently, the 1.2V, 3.3V and internal 1.8V power supplies of the MCU are all functioning normally.